This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: 按SW21开关按钮,电路板有反应,但无法开启投影仪

Part Number: DLP4710EVM-LC

您好!
我们实验室购买了一台DLP4710EVM-LC,刚开始是可以正常工作的,使用期间我们按照TI给的使用手册进行烧录数据,投影操作。
但目前,该投影仪无法正常工作了,其现象为:移动SW28 (PS_ON/OFF)滑动开关到ON位置,led D43 (+3.3V)和D57 (INTZ)亮起。按下开关SW21打开DLP4710EVM时,led D36 (SYS_ON-OFF), D33 (M_IRQ)和D34 (S_IRQ)不再亮起。另外,当按下开关SW21时,D56亮-灭一次,D57灭;松开开关SW21时,D56亮-灭一次,D57亮。
请问这种情况是什么原因?如何解决?
期待您的回答,祝您生活愉快,工作顺利。