最近想开发一款1280x720的200lm的DLP微型投影,光引擎部分已经选好正在确定驱动芯片方案,有几个问题想咨询一下。
1关于DLPC的选型,看到了TI提供的直接配套的控制芯片是DPP3433和DPP3438,这两款芯片的管脚除中心的25个接地管脚外完全一样,除了尺寸以外,这两款芯片有什么区别吗?
2我购买了几款光引擎厂商提供的DEMO机,发现有的厂家使用了DPP3435来控制720P的光机,那么DPP3433与DPP3438有没有控制未来1080P的DLP4710的能力?
3关于DLPA的选型,我拆解了几款demo机,他们的亮度在200lm以上,光机驱动电流平均在3-4A,但他们都使用了PAD2005芯片驱动。我查看了PAD2005的资料发现他的驱动电流最高到2.6A,不能达到驱动标准,有的厂家使用了外接降压转换器的方式来驱动LED。那么如果使用PAD3000的话,它的驱动电流是6A,那么是不是就可以直接驱动LED了,另外PAD2005能否直接驱动200lm的光机(电流最大值4A)呢?
4看到DLPC需要外接一个Flash,这个Flash是存储什么的?另外DLPC里面有许多寄存器需要配置,使用什么方式进行配置呢?
5要设计一个光引擎的驱动和HDMI解码都需要那些方面的技术储备?