This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DLP驱动的Flash与PAD3000电源管理

Other Parts Discussed in Thread: DLPA3000

现在已经确定了DPP3433+PAD3000的主芯片方案,看到TI官方的EVM模块的Flash使用了16M的,我拆解的其他厂家的驱动有使用32MFlash的,那DPP3433使用的Flash最小能使用多大的?

Flash里面存储的固件是使用类似msp430一类的单片机通过IIC接口与SPI接口烧写进去的吗?还是其他方式?需要什么烧写工具吗?

Flash里面的固件是用什么语言写的呢?使用的什么编译环境?有源码可以参考吗?

看到参考原理图里面DPP3433需要四个电源,1.8v、1.1v、3.3v(核心)、3.3v(VFLSH),其中PAD3000可以提供前三个电源,第四个是外接的降压转换器。那这个VFLSH一定要使用单独的电源芯片吗?可不可以使用PAD3000供电?可不可以与核心的3.3v接在一起?

  • 1、最小可以使用16M bit的。

    2、通常是通过普通的SPI烧录器直接烧录到Flash芯片里。

    3、Flash里面的固件是二进制文件,用Composer工具进行编译而成,一般由光学模块厂家提供。

    4、3.3V供电可以直接由DLPA3000产生,即整个板子只需要输入一个主电源就可以了。