This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3433: DLPC3433 配置DSI出现无法显示图现象(花屏)

Part Number: DLPC3433

mipi配置
1280x720@60Hz
MIPI Timing
#define PANEL_FRAME_RATE 60
#define PANEL_H_ACTIVE 1280
#define PANEL_V_ACTIVE 720
#define PANEL_VFP 5
#define PANEL_VSYNC 5
#define PANEL_VBP 20
#define PANEL_HFP 110
#define PANEL_HPW 40
#define PANEL_HBP 220

dlpc寄存器配置
1a 01
d7 00
10 00 00 00 00 00 05 d0 02
12 00 00 00 00 00 05 d0 02
2e 00 05 d0 02
bd df 00
05 00
07 00
14 02
1a 00

目前是出现在平台初始化完成以后 模块0x07寄存器读出来的值是0x00 这个值应该是异常的

息屏 在亮屏出现花屏 现象是慢慢刷屏 覆盖马赛克。

请TI帮忙看下,谢谢。