DLP3010: DLP3010显示异常

Part Number: DLP3010
Other Parts Discussed in Thread: DLPC3433, DLPA2000,

您好:

我在使用DLP3010+dlpc3433+dlpa2000的方案时,遇到一些问题:

1:在无外部视频输入时,使用内部测试图片,显示一切正常,当我使用外部视频输入时,一开始也是正常的,当我持续使用外部视频输入的时候,大约过个几分钟或者十几分钟(时间不固定,未使用温度传感器,以及系统温度不高),画面会消失(无画面输出),但是led还是持续亮着。如果我重新通电,还是会正常显示几分钟后无画面输出,请问这是什么原因造成的。

2:FWSel_DLPC3433_AR_DLPA2000固件与FWSel_DLPC3433_DLPA2000固件两者的区别具体是什么。

谢谢