This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP LightCrafter 实现0-1小数级别的控制



我买的器件是DLP LightCrafter。一般DMD都是0-1序列或者图像对DMD镜片进行控制,但是我想用DMD实现小数。具体的说,在这个时钟周期内,对于某两个镜片对应的控制系数是0.3和0.5(控制系数的范围是0到1之间),我就让这两个镜片在一个时钟周期内分别有30%和50%的时长将光线反射到探测器中被采集到;而对于下一个时钟周期,这两个镜片对应的控制系数就会改变,假如说0.8和0.1,就按照上述方法来实现。请问 lightcrafter可以实现这种控制吗?  其实关键问题是,在一个时钟周期内我可不可以只对某些镜片进行控制让其翻转?