我参考了DLPC3435,DLPC3438,DLPC3439的官方EVM原理图,发现VCC_INTF的供电电压不同,DLPC3435与DLPC3438的INTF供电是1.8V的,而DLPC3439的供电是3.3V的。datasheet中VFLSH与VCC_INTF都是可选1.8V或3.3V供电的,这两种供电有什么区别?怎样选择供电电压,是需要配置寄存器还是,自动识别的?DLPC3435和DLPC3438的VFLSH与INTF通常应该供多大电压?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
VFLSH是给SPI Flash芯片的供电,不同型号的flash电压可能会不同,常用的是1.8V和3.3V。VCC_INTF是前端视频信号的电压幅度,通常为3.3V。这两个电压都是硬件设计决定的,和寄存器设置无关。