Other Parts Discussed in Thread: DLPA2000, DLPC3435
使用DLPC3435和DLPA2000做了一个驱动电路,在没接光机的时候上电测试,发现如下问题
1,原本干净的系统电源出现了振幅1V,频率1KHz的纹波,在系统电源并联电容有有好转,但依旧有0.5V的纹波。那么系统电源的电容应该加到多少?为什么会出现这样的纹波?
2,DLPA2000发热严重,上电几秒种后,DLPA2000就开始有些烫手了,这是什么原因?需要给DLPC2000安装散热器吗?
3,经过测量,给DLPA2000供电的系统电源有纹波,1.8V电源质量较好;在没有安装配置Flash芯片时DLPA2000能够输出1.8V,2.5V电源,VCORE有非常大的纹波,平均值在0.5V左右:在安装Flash(没接光机DMD)时能够输出1.8V,2.5V,VOFS(5V),VBIAS(5V),VCORE仍然有非常大的纹波,平均值在0.5V左右。那么VCORE为什么没有输出正常的1.1V电源?是和系统电源质量不好有关系吗?
4,如何判断DLPA2000是否损坏?
谢谢