This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tl16c754c接收数据出错

我用了s3c2410外扩了4个串口,用的是tl16c754. s3c2410的D0~D7接754的D0~D7,s3c2410的读使能和写使能分别接754的读使能和写使能。现在遇到的问题是,通过PC机给某一路发送数据,字节数过多时,一般28个字节之后就全是乱码了,不知道怎么解决。

  不过,我尝试过,将计算出来的分频值减去1之后再写���DLL和DLM,接收数据正常;或者将PC机的串口调试助手停止位设为2,754接收数据也没问题。但这些毕竟没有彻底解决问题!

  另外,发送数据没有问题,754的串口之间发送、接收也没有问题,但就是外部发来的数据不能正确接收

  在754端晶体用了3.6864MHz,两个腿接的电容都是22pF,晶体工作正常,也比较稳定。

  我用了外部中断,中断方式接收数据。

      ChangeClockDivider(1,0);        // 1:2:2    

  ChangeMPllValue(0xa1,0x3,0x3);  // FCLK=50.7MHz  

//        总线初始化 BANK3

      rBWSCON=rBWSCON& (~(0xf<<12))|(0<<12);// |(1<<14)|(1<<15)

      rBANKCON3=0x5650;

  Port_Init();                                        // 初始化I/O口

  Isr_Init();

/***************        TL16C754中断管脚定义        *****************/

      rGPGCON &= ~((3<<0)|(3<<2)|(3<<4)|(3<<6)|(3<<8)|(3<<10)|(3<<12)|(3<<14));

      rGPGCON |=        ((2<<0)|(2<<2)|(2<<4)|(2<<6)|(2<<8)|(2<<10)|(2<<12)|(2<<14));        

                                                                      //GPG0 ~ 7 set eint8 ~ 15

      rEXTINT1 &= (~((7<<0)|(7<<4)|(7<<8)|(7<<12)|(7<<16)|(7<<20)|(7<<24)|(7<<28)));

      rEXTINT1 |= ((4<<0)|(4<<4)|(4<<8)|(4<<12)|(4<<16)|(4<<20)|(4<<24)|(4<<28));                

                                                                      //set eint rising edge int

      rEINTPEND |= (1<<8)|(1<<9)|(1<<10)|(1<<11)|(1<<12)|(1<<13)|(1<<14)|(1<<15);                //

      rEINTMASK &= ~((1<<8)|(1<<9)|(1<<10)|(1<<11)|(1<<12)|(1<<13)|(1<<14)|(1<<15));        //

                                                                      //enable eint8~15

      ClearPending(BIT_EINT8_23);

      pISR_EINT8_23 = (U32)Uart_RxInt;        

      rINTMSK &= ~(BIT_EINT8_23);                // 开中断

//        rPRIORITY &= ~(3<<9);                        // 设定中断优先级

/****************        TL16C754复位                **********************/

      rGPFDAT &= ~(1<<7);

      Delay(100);

      rGPFDAT |= (1<<7);

      Delay(200);

      rGPFDAT &= ~(1<<7);

/****************        TL16C754初始化                **********************/

      for( ch=0; ch<8; ch++ )        

      {

              writeb( pEXT_COM_BASE_ADDR[ch]+LCR, 0x80 ); // when LCR b7 is 1, DLL & DLH are accessed

              writeb( pEXT_COM_BASE_ADDR[ch]+DLH, (BaudRateTab[3]>>8)&0x00ff );

              writeb( pEXT_COM_BASE_ADDR[ch]+DLL, BaudRateTab[3]&0x00ff );

              writeb( pEXT_COM_BASE_ADDR[ch]+LCR, 0x03 ); // 8-bits 1-stop no-parity

              writeb( pEXT_COM_BASE_ADDR[ch]+FCR, 0xc7 );        // c7

              writeb( pEXT_COM_BASE_ADDR[ch]+IER, 0x01 ); //0x01 enable receive interrupt

              writeb( pEXT_COM_BASE_ADDR[ch]+IIR, 0x01 );

              writeb( pEXT_COM_BASE_ADDR[ch]+MCR, 0x00 ); // 08

              Delay(1);        

      }

      while(1)

      {

              if( (NumOfUartRxInt>0)&&(NumOfUartRxInt<9) )

              {

                      temp = readb( pEXT_COM_BASE_ADDR[(NumOfUartRxInt-1)]+IIR );

                      temp = temp&0x3f;

                      if( (temp==0x0c)||(temp==0x04) )

                      {

                              temp1 = readb( pEXT_COM_BASE_ADDR[(NumOfUartRxInt-1)]+LSR );

//                                if( temp1&0x1)

                              {        

                                      RecData = readb( pEXT_COM_BASE_ADDR[(NumOfUartRxInt-1)]+RHR );

                                      writeb( pEXT_COM_BASE_ADDR[(NumOfUartRxInt-1)]+THR, RecData );

                                      NumOfUartRxInt = 0;

                                      RecData = 0;

                              }

                      }

              }        

      }

我用串口调试助手发送了一串‘66666666666666……’,16c754接收之后再发送出去,调试助手显示如下:

36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 96 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 9B 4F 4D 4D 4D 4D 4D 4D 4D 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 93 CB C9 C9 C9 C9 C9 C9 C9 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 B2 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 D9 6C 6C 6C 6C 6C 6C 6C 6C 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 36 B6 9B 9B 9B 9B 9B 9B 9B 9B

用9600bps发送数据时,测得实际的波特率大概是9540,误差比较大。换过几个晶体,也调节过晶体的输出频率,初步确定应该不是因为晶体的精度不够才造成的这个现象。

不知有没有遇到这种情况的,如何解决……期待解答

  • 你好!

    为了确保可靠通信,一般要求波特率相对误差不大于2.5%。而在这个电路中是9540的波特率应该还是可以保证可靠通讯的。

    如果你想测试16c754能否接收数据的话,建议首先建立一定的通讯协议,有帧头帧尾字长即可,可以使用串口助手发送给16c754,若16c754接收数据正常的话,那么可以通过硬件给予一个亮灯信号灯,或者上传一个1给串口助手(否则一直上传0)。你的这种简单的大批量数据上传的话,不光要考虑16c754能否正常接收,还要考虑上位机的缓存是否够用,中间是否存在干扰,在这种没有协议的通讯中,如果丢失任何一位,后面基本上都是乱码。

    谢谢!

  • 问题解决了吗?我也遇见这样的问题了,故障现象相同,不同的是,CPU是LPC2294。