This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC1004液位探测芯片相互干扰的问题

TI的各位专家;

      你们好,我司在使用TI的FDC1004液位探测芯片做液位探测时,出现了如下问题:

       1、设置数据输出速率为400S/s,然后用示波器测量芯片的输入引脚和屏蔽引脚发现有固定频率的激励信号,频率大概为250KHZ,,在一块液位探测板单独供电时检测数据正常,但是同时上电就会出现有规律的高频干扰叠加在检测信号上,严重影响了正常液位监测。如果将其中一个板子断电或拔掉信号输入线,噪声消失。分析为该固定频率激励信号造成了两块液位探测版相互影响。因为我司设计的产品由于结构要求,信号输入引脚分别链接到一个管状针上,并且针内填充有浓度较高液体,通过针尖接触其他液面进行液位探测。结构要求针内填充的液体必须物理连接,分析干扰是通过针内高浓度液体进行传导。请问有什么好的方法可以屏蔽掉这个高频噪声?

        2、由于我司产品结构决定了其基础电容值较大,部分产品超过120PF,不能通过差分或设置偏移量对其进行检测,超出了FDC1004的监测范围,请问TI有没有检测范围更大的芯片以供采购。

        望解答,谢谢。