Part Number: TUSB2046B
1:根据这份文件Application Report SLLA314,USB信号线TI建议串联阻抗匹配电阻,请问TUSB2046BI这颗HUB的内阻多大?需要串联多大阻值的电阻?谢谢!
2:请问晶体的频率是否只能选择6MHz这个频率?我们的空间有限,6MHz的晶体体积过大。其他比如8MHz、12MHz是否可以?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB2046B
1:根据这份文件Application Report SLLA314,USB信号线TI建议串联阻抗匹配电阻,请问TUSB2046BI这颗HUB的内阻多大?需要串联多大阻值的电阻?谢谢!
2:请问晶体的频率是否只能选择6MHz这个频率?我们的空间有限,6MHz的晶体体积过大。其他比如8MHz、12MHz是否可以?

您好,
根据这份文件Application Report SLLA314,USB信号线TI建议串联阻抗匹配电阻,请问TUSB2046BI这颗HUB的内阻多大?需要串联多大阻值的电阻?谢谢!
这是一款非常旧的器件、我们没有用于检查内部电阻的设计资源。
请问晶体的频率是否只能选择6MHz这个频率?我们的空间有限,6MHz的晶体体积过大。其他比如8MHz、12MHz是否可以?
对于晶体,只有 6Mhz 有效,您也可以向 XI 引脚提供外部 48Mhx clk。