LMK5B33414 XO输入48MHZ(±50ppm),IN0输入25MHZ(±10ppm),LMK5B33414工作在抖动衰减藐视 ,OUT0输出312.5M时钟,312.5M时钟精度是±50ppm?还是±10ppm?怎样计算的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LMK5B33414 XO输入48MHZ(±50ppm),IN0输入25MHZ(±10ppm),LMK5B33414工作在抖动衰减藐视 ,OUT0输出312.5M时钟,312.5M时钟精度是±50ppm?还是±10ppm?怎样计算的?
您好,
数据表在8.2.2 DPLL 部分中对此进行了说明。
"
When DPLL operation is enabled and the DPLL is locked, the DPLL reference inputs (INx pins) determine the frequency stability and accuracy of the output clocks. The clock source on the XO pin determines the free-run and holdover frequency stability and accuracy of the output clocks. The VCBO determines the BAW APLL output clock phase noise and jitter performance over the 12kHz to 20MHz integration band, regardless of the frequency and jitter of the XO pin input.
"