TI高工你好,我现在的应用是ARM->UB927->UB928->LVDS屏+CTP。有几个问题需要麻烦高工们帮我解惑下:
1.目前图像传输过来是180反的,想问问串行器和解串器能否把图像rotator弄成正常,这样的话更改工作最小。
2.I2C PASS ALL是不是允许所有I2C通讯,类似于I2C PASS THROUGH+SlaveID和Slave Alias的过滤效果。问题
(1) 我目前的情况是不开UB927的I2C PASS ALL,linux的I2C总线没法识别到UB928,用demo板是不用设置I2C PASS ALL可以P读取UB928的寄存器,那说明路是通的。
(2)同样的情况我可以用外挂i2c master 通过UB927->UB928 操作触摸屏的I2C寄存器,但是linux的I2c总线就是识别不到,是不是需要什么设置?还是是我linux驱动的问题?