This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1310的差分对正负之间是否可以交换?

Other Parts Discussed in Thread: TUSB1310, TUSB3410

问题如题。 如果不能交换,数据手册37页这段话是啥意思? 谢谢!

It is permissible to swap the plus and minus on either or both of the SuperSpeed differential pairs, which may be necessary to prevent the differential traces from crossing over one another. However, it is not permissible to swap the transmitter differential pair with the receive differential pair.

  • 这里的意思是正负差分对间可以交换,因为有时候PCB layout时不方便布线,不得不将发送和接收差分对间的“+”“-"交换,防止布线交叉。

    但是不允许的是发送和接收的差分对之间互相交换,也就是说发送端当做接收端,接收端当发送端。

  • Hi Kailyn,你的意思是TUSB1310支持差分线对的正负交换? 因为其它家的这个产品是没有这个功能的。 我觉得上面这段话放在PCB layout这段里面, 应该不是芯片本身属性的描述, 麻烦确认一下。 谢谢!

     

  • 不光TUSB3410这一款,任何差分对间的正负都可以交换,只要保证对应关系就好,可以看下datasheet Page 34的图更直观一些,可以看到RXP和connector端的RXN连,RXN个connector端的RXP连,同样,TXP和TXN也对应的connector 端的TXN和TXP,这样是没问题的。

  • Hi Kailyn,

           我就是被这个图搞糊涂了。 这样说吧,对端芯片的TXP/TXN, 跟TUSB1310的连接关系是RXP/RXN还是RXN/RXP? 还有这个芯片只有TX做了AC耦合, RX需要AC耦合吗? 谢谢!

  • 对端芯片的TXP/TXN, 跟TUSB1310的连接关系是RXP/RXN还是RXN/RXP? 

    A:对端芯片的TXP/TXN, 跟TUSB1310的TXN/TXP 都能连接,那么相应的对端芯片的RXP/RXN也跟TUSB1310的RXN和RXP连接。

    就是说如果TX正负反接,那么RX正负也反接就行了,

  • 还有这个芯片只有TX做了AC耦合, RX需要AC耦合吗?

    A: datasheet中有对这个做了描述,只有TX差分对上需要。

    The transmitter differential pair requires 0.1-μF coupling capacitors for proper operation. The package
    or case size of these capacitors must be no larger than 0402. C-packs are not allowed. The capacitors
    must be placed symmetrically as close as possible to the USB connector signal pins.