Part Number: DP83640
在使用page4的0x14和0x15进行load lck和rd clk时,是否需要考虑mdio命令的读写时间,例如在load clk时,是在0x14[4]写入为1时生效,但此时距离写入ns时间已经过去了四个mdio命令时间,生效的时间不就慢了这么长时间?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你们计划如何处理第4页寄存器0x14和0x15?你们是否尝试从DP83640读取时间戳以实现同步?
DP83640已经集成了1588功能,使系统设计人员能够实现接近线时间戳的灵活性和精度。该设备支持的三个关键1588功能是:
• Packet time stamps for clock synchronization
• Integrated IEEE 1588 synchronized clock generation
• Synchronized event triggering and time stamping through GPIO