因为外设是类似camera设备,外设电平在3.3V,CPU电压是1.8V,所以需要电平转换,器件官方要求转换速率要大于150Mbps才能正常工作,TI工程师能否推荐一颗适合的电平转换芯片,最好是不需要DIR方向控制的,直接双向
另外:不要推荐TXB01xx之类的,看过了手册了,VccA在1.8V时,最高速率只能到60Mbps,根本不行。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因为外设是类似camera设备,外设电平在3.3V,CPU电压是1.8V,所以需要电平转换,器件官方要求转换速率要大于150Mbps才能正常工作,TI工程师能否推荐一颗适合的电平转换芯片,最好是不需要DIR方向控制的,直接双向
另外:不要推荐TXB01xx之类的,看过了手册了,VccA在1.8V时,最高速率只能到60Mbps,根本不行。
需要几个bit的?不带方向控制位的目前只有TXS010xx和TXB010x系列两大类。
可以考虑16bit SN74AVC16T245, 1.8V到3.3V转换能够支持380 Mbps data rate.
不过这颗是带方向控制位的,不知是否满足你的要求