This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

采用 TUSB8041设计USB3.0 hub,但调试时插入USB3.0硬盘,主机没有任何反应

Other Parts Discussed in Thread: TPS65286, TUSB8041, TPS2561

TI的工程师您好,

我采用 TUSB8041并按照数据手册的参考设计设计了四端口USB3.0 hub,采用TPS65286搭成24V to 5V(6A)的输出供给下行端口的port1、port2、TUSB8041的1.1V、3.3V及TPS2561(用于下行端口的port1、port2电源管理),但调试时在hub的下行端口插入USB3.0硬盘,主机没有任何反应,但硬盘会正常振动。当同时在hub的下行端口插入USB 2.0的优盘,主机就可以正常识别2.0的优盘。另外硬盘直接插到主机的USB3.0口(不采用hub时)主机是可以正常识别的。

请问是下行端口供电不足导致的吗?

还是TUSB8041要工作在3.0模式下还需进行相关的配置?

还是其他的什么原因呢?

期待您的回答,谢谢!

x 出现错误。请重试或与管理员联系。