Part Number: DS90UB662-Q1
If the TFT resolution is 2560 × RGB × 1440 @ 60Hz, can DS90UB688 be used?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB662-Q1
If the TFT resolution is 2560 × RGB × 1440 @ 60Hz, can DS90UB688 be used?
A video signal for a 2560x1440 @ 60 Hz resolution would have a PCLK that is too large for the UB688. The UB688 has a max PCLK of 210 MHz with dual link and your resolution and refresh rate would require at least 220+ MHz depending on the blanking required for your panel. You can either drop the refresh rate to something like 30 Hz to lower the PCLK, or you can go with a device that can use higher PCLKs such as the UB988.