This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
12脚复位引脚是输入引脚,不是输出,上电之后,它是一个由低到高的变化过程,power稳定之后,RST由低拉高。 可以用主控去控制。
现在复位是正常的,管脚23----OSCOUT也有25M的波形输出,为什么 2,3管脚还是没有波形????
管脚10,11,13,14,15,25,26的值是什么?测试的结果是什么?
Seasat Liu 感谢您的回答,现在的值 26---0 ,25---0,15---1 ,14---0, 13---1 ,11---1,10---0
测试的结果没有时钟输出
控制输入端CE和OS1,OS0都是给的什么电平?输出使能端 CE高有效。fanglei zhao 说:现在复位是正常的,管脚23----OSCOUT也有25M的波形输出,为什么 2,3管脚还是没有波形????
OS1,OS0都是给的1,0 和0,1都试过,CE现在上拉10K的电阻,是高电平
我算的结果是
CE=1
RSTN=1
OS1=OD0=0
PR0=PR1=0
OD0,OD1,OD2=101
电路没什么问题,还是需要验证两点:
CE高电平,Vih(min)不能低于0.6Vcc即1.98V。
另外,还是再验证下reset时序,当power和CE都为高电平稳定之后,reset再由低为高。
reset这个信号有照示波器抓了下,应该是对的,CE现在的电压3.3V