Part Number: DS90UB988-Q1
Hello expert, When we want to use the two daisy chain outputs of 988 to simultaneously transmit to two different 928,Do we need 988's input terminals to also have two inputs (RIN0/RIN1) when transmitting the two daisy chains on 988 to the next level? If there is only one input, does it support two daisy chain outputs?