This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: TECHNICAL SUPPORT

Part Number: DS90UB953-Q1

HI

 

 

 

I'd like to inquire about technical support for the DS90UB953-Q1 IC, which is scheduled to be used in the LGD VH Ultra-Large Auto Chamber Wing Board (requesting confirmation of contact point).
 
Inquiry
 
1. Device Part: TI's "DS90UB953-Q1" FPD Link IC (scheduled for future ultra-large chamber wing boards)
 
2. Inquiry
 
1) The HPD signal of the "DS90UB953-Q1" IC swings when the screen doesn't operate.
 
-> We need to check the conditions under which the HPD signal swings.
 
-> Based on the attached circuit diagram, the "HPD" signal on Pin 64 swings.