This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SERDES 芯片 953 960

听别人说起SERDES 953和960但不知具体型号,有谁知道具体型号和相关资料吗,据说960可接4路输入

  • 应该是DS90UB953, DS90UB960这两款。

  • 您好,

    型号是DS90UB953和DS90UB960,是下一代产品,目前还没有量产,960可以接4路输入。目前量产的针对Camera的FPD-Link Serdes 产品是DS90UB913和DS90UB914.

    Kevin

  • 现在有DS90UB953和DS90UB960的资料吗?不久就要使用这两款芯片了,想先了解一下。

    另外问下:最近做了一套POC 的camera module+913+914+FPGA的case, 1280x800 DVP 72M 12bit MODE,,913输入DVP 信号一直有的但914端LOCK 信号一直低,仔细check 了913和914的原理图发现POC电路有个100uH和5.6uH的电感,DS上推荐colicraft 4.7uH, 但是即使914和913端都将此换成4.7uH仍然没效果, 但当913 4.7uH,914 5.6uH时偶尔有LOCK 信号,也考虑过阻抗匹配问题, 减少913端输入功耗,减小resolution但LOCK 信号一直不稳定,这是什么原因呢?难道与PCB layout 有关?求解!这个问题搞很久了~~

  • 目前还没有DS90UB953和DS90UB960的资料可以参考,如果有的话,在官网是可以直接搜索到的。

  • 关于LOCK问题,建议测量下PDB和LOCK的时序问题,当PDB由低为高之后,最大需要22ms的时间lock才由低变高。参考Figure12.

    另外,还是要注意下上电时序问题,当VDDIO和VDD_core电压由低到高稳定之后,PDB再拉高。