Other Parts Discussed in Thread: TSS521
客户使用TSS521进行一对一通讯,由主设备给从设备供电;
1.芯片VDD管脚最大输出电流10mA,VDD管脚输出电流能否调节?
如果可以调节,在0-10mA范围内任意调节,能否正常通讯?
2.正常使用时,BUSL1,BUSL2两路电压分别为36V,24V,压差为12V,
如果改变BUSL1,BUSL2上电压,但保持两线压差为12V,能否正常
通讯?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TSS521