Other Parts Discussed in Thread: SN65DSI84, SN65DSI83
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN65DSI84, SN65DSI83
你好,
请用高速示波器测量一下输入信号的抖动,眼图是否合格,各并行信号间的skew是否符合要求, 电缆及连接器的质量是否达标,DSI84的供电噪声是否正常。 总之,我比较怀疑是输入信号质量不好造成黑屏。
你好,
目前缺少高速示波器测量,MIPI信号源与DSI84芯片在同一块PCB板上,信号输入线都有进行100欧姆差分阻抗控制,参考地平面完整,PCB布线方面可以说是不存在问题,供电采用LDO,纹波噪声在20mV以下。不理解的是不管黑屏还是正常,0xe5寄存器读值均为0x01(PLL_ULOCK),如何才能实现读值为0x00?黑屏时,0xe5读值出现其它数值也是一个较小的概率,如果是DSI信号问题,为何0xe5寄存器报错基本上是不准的?
你好,
由于黑屏不是每次都出现,所以e5寄存器也不是每次都报错。报错的时候已经是比较严重的问题了,加之报错时信号出问题只是在DSI84本身及其前端,此信号传输到屏上时信号质量会更差,造成屏端解码芯片更加无法解码,所以黑屏。 就像你说的,信号质量跟PCB布局有关,但跟MIPI信号源的质量也有很大关系,比如MIPI源的时钟不干净,电源不干净,或者其他信号干扰,都会造成信号抖动过大而造成e5报错。 因此我还是建议你检查信号源的抖动情况,并实际测量给DSI84的供电已经MIPI信号源芯片的供电以及时钟抖动,不然我们用其他方式更加难以定位问题。
还有一半办法来验证是不是信号质量的问题:请把分辨率降低,看是否还黑屏,如果不黑了,说明是信号质量问题,原因是低分辨率对信号噪声的容忍度会显著增强
经过试验,基本解决了反复开关机概率性黑屏的问题。目前试验了上万次,未再发现SN65DSI84初始化失败的问题。原因确实是由于程序初始化流程问题,须严格遵守datasheet中描述步骤。证明了硬件设计,包括PCB是没有问题的。SN65DSI84对PCB布线的要求也没有传说的那么“高”。我们先后设计制作了三种MIPI->LVDS方案,TI的方案除了调试困难,其性能和转换后的图像质量确实无可挑剔。有点儿小贵。
以下是1080p屏上用过的一组配置,你根据自己的屏改一下FP/BP/SYNC值后试试!
ret = sn65dsi83_regw(i2c, 0x09, 0x01);
if(ret < 0)
return;
//PLL_EN(bit 0) - Enable LAST after addr 0A and 0B configured
sn65dsi83_regw(i2c, 0x0D, 0x00);
msleep(10);
//HS_CLK_SRC bit0
//LVDS_CLK_Range bit 3:1
// sn65dsi83_regw(i2c, 0x0A, 0x04);
//DSI_CLK_DIVIDER bit7:3
//RefCLK multiplier(bit1:0)
//00 - LVDSclk=source clk, 01 - x2, 10 -x3, 11 - x4
// sn65dsi83_regw(i2c, 0x0B, 0x00);
//DSI Ch Confg Left_Right Pixels(bit7 - 0 for A ODD, B EVEN, 1 for the other config)
//DSI Ch Mode(bit6:5) 00 - Dual, 01 - single, 10 - two single
//SOT_ERR_TOL_DIS(bit0)
sn65dsi83_regw(i2c, 0x10, 0x26); //use 4 lanes DSI
// sn65dsi83_regw(i2c, 0x11, 0x00);
sn65dsi83_regw(i2c, 0x12, 0x57); //DSI CLK 411MHz
// sn65dsi83_regw(i2c, 0x13, 0x00);
//bit7: DE_Pol, bit6:HS_Pol, bit5:VS_Pol, bit4: LVDS Link Cfg, bit3:CHA 24bpp, bit2: CHB 24bpp,
//bit1: CHA 24bpp fmt1, bit0: CHB 24bpp fmt1
sn65dsi83_regw(i2c, 0x18, 0x6C); //use 4 lanes LVDS
sn65dsi83_regw(i2c, 0x19, 0x0F);
sn65dsi83_regw(i2c, 0x1A, 0x03);
// sn65dsi83_regw(i2c, 0x1B, 0x00);
//CHA_LINE_LENGTH_LOW 1280
sn65dsi83_regw(i2c, 0x20, 0x80);
//CHA_LINE_LENGTH_HIGH
sn65dsi83_regw(i2c, 0x21, 0x07);
//CHA_VERTICAL_DISPLAY_SIZE_LOW 720
// sn65dsi83_regw(i2c, 0x22, 0x00);
// sn65dsi83_regw(i2c, 0x23, 0x00);
// sn65dsi83_regw(i2c, 0x24, 0x00);
//CHA_VERTICAL_DISPLAY_SIZE_HIGH
// sn65dsi83_regw(i2c, 0x25, 0x00);
// sn65dsi83_regw(i2c, 0x26, 0x00);
// sn65dsi83_regw(i2c, 0x27, 0x00);
//CHA_SYNC_DELAY_LOW
sn65dsi83_regw(i2c, 0x28, 0x20);
//CHA_SYNC_DELAY_HIGH
// sn65dsi83_regw(i2c, 0x29, 0x00);
// sn65dsi83_regw(i2c, 0x2A, 0x00);
// sn65dsi83_regw(i2c, 0x2B, 0x00);
//CHA_HSYNC_PULSE_WIDTH_LOW
sn65dsi83_regw(i2c, 0x2C, 0x04);
//CHA_HSYNC_PULSE_WIDTH_HIGH
sn65dsi83_regw(i2c, 0x2D, 0x00);
// sn65dsi83_regw(i2c, 0x2E, 0x00);
// sn65dsi83_regw(i2c, 0x2F, 0x00);
//CHA_VSYNC_PULSE_WIDTH_LOW
sn65dsi83_regw(i2c, 0x30, 0x04);
//CHA_VSYNC_PULSE_WIDTH_HIGH
sn65dsi83_regw(i2c, 0x31, 0x00);
// sn65dsi83_regw(i2c, 0x32, 0x00);
// sn65dsi83_regw(i2c, 0x33, 0x00);
//CHA_HOR_BACK_PORCH
sn65dsi83_regw(i2c, 0x34, 0x82);
// sn65dsi83_regw(i2c, 0x35, 0x00);
//CHA_VER_BACK_PORCH
// sn65dsi83_regw(i2c, 0x36, 0x00);
// sn65dsi83_regw(i2c, 0x37, 0x00);
//CHA_HOR_FRONT_PORCH
// sn65dsi83_regw(i2c, 0x38, 0x00);
// sn65dsi83_regw(i2c, 0x39, 0x00);
//CHA_VER_FRONT_PORCH
// sn65dsi83_regw(i2c, 0x3A, 0x00);
// sn65dsi83_regw(i2c, 0x3B, 0x00);
sn65dsi83_regw(i2c, 0x0A, 0x05);
sn65dsi83_regw(i2c, 0x0B, 0x28);
sn65dsi83_regw(i2c, 0xE0, 0x01);
//Clear all error code
sn65dsi83_regw(i2c, 0xE5, 0xFF);
//PLL_EN(bit 0) - Enable LAST after addr 0A and 0B configured
sn65dsi83_regw(i2c, 0x0D, 0x01);
msleep(10);
//SOFTRESET
sn65dsi83_regw(i2c, 0x09, 0x00);