我有一客户很早有用TMDS361,20dB,3Gbps时,可以做到40米,现在因为它停产了,建议客户换成TMDS361B,客户拿了样品直接换上去做测试,发现效果很差,而且只能做到30米。客户希望TMDS361B 也能支持HDMI线缆到40米,而且是越长越好。
规格书上只写能支持到20m,客户说那是用眼图测试的,如果用电视测就能40米,就是实际使用可以达到40米。
请问:新版TMDS361B 的应用图纸要怎么改?才能做到和停产版TMDS361一样甚至更长的长度呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
换成TMDS361B,测试条件完全一样?
一般都是测试眼图,用电视测不是看眼图吗?效果差是指jitter很大吗?
Kailyn,你好!
客户是测试的延长距离,老版本TMDS361跟新版本TMDS361B都是最大距离20dB,测试条件和原理图都是一样的,为什么新版TMDS361B延长的距离要短很多呢?