用SN65DSI86 成功使液晶屏顯示了,然後往DSIx6的0xc8寄存器寫入值0X02,沒有任何反應。請問怎麼使能PSR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是能PSR条件如下:
1. Updates to the remote frame buffer located in sink must include two of the same static frame. The reason for
this requirement is the DSIX6 will never pass the first frame received on the DSI interface to the DisplayPort
interface. All subsequent frames will be passed to the DisplayPort interface.
2. If PWM signal is controlled directly by the DSIX6 and SUSPEND asserted, the REFCLK must remain active.
3. Changes in ambient light level must be relayed to the DSI96 along with updates to the remote frame buffer in
the sink.
4. Sink CRC verification must be disabled when the Assertive Display core is enabled. (applies only to the
SN65DSI96)
首先需要满足以上条件,然后再试试是能寄存器。