TMDS181RGZEVM: How to used the TMDS181 as a sink side EQ part at 4K/60? I want to know the hardware degin and the register set of the chip.

Part Number: TMDS181RGZEVM
Other Parts Discussed in Thread: TMDS181, TDP1204

  1. We use the   TMDS181 as  a  sink  side  EQ   part  at 4K/60. But  only  support  4K/30.
  2. We use the   TMDS181 as  a  source  side    part  at 4K/60. But  nothing  out .
  3. I  want to know the  hardware degin  and   the  register  set  of  the   chip  while  it used as a sink side or a source side .

                                                                                                             Thank you  very much!

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 您好

    对于将 TMDS181 用作灌电流器的情况,请确保 I2C_EN 具有 65k 上拉电阻和 10k 下拉电阻。请将 EQ_SEL 和 TX_TERM_CTRL 悬空。SPDIF_IN 需要 500k 下拉电阻。SDA_SRC 和 SCL_SRC 需要 47k 上拉电阻至 5V,请检查 SDA_SNK 和 SCL_SNK 上的上拉电阻值。

    他们是否通过寄存器手动配置了 TMDS181?对于 4K@60(即 HDMI 2.0),寄存器 0x​​0B 的第 1 位 TMDS_CLOCK_RATIO_STATUS 必须为 1。但 TMDS181 应该根据 DDC 侦听自动设置该值。

    源端使用的是TMDS181还是TDP1204?如果是TDP1204,AC_EN引脚是拉低还是拉高?

  • 您好!

           非常感谢您的帮助。我们正在按照您的已经进行排查。

            另外,有个问题需要麻烦您核实一下:

            您问的:源端使用的是TMDS181还是TDP1204?是指我们使用的HDMI信号源的输出端口的芯片使用情况吗?谢谢!

        

  • Hi:

        Thank you very much for your help. We'll  debug  it  as your  suggest.

        There  are  some thing to Confirm : The source  you enquired use TMDS181 OR  TDP1204  wheater  refer to the equipment  of the       HDMI Generator?

        Thank  you very much!

  • 您好

    我问TMDS181或TDP1204是在PC、笔记本电脑或HDMI发生器等源中设计的,还是在显示器等接收器中设计的。