This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CDCE62005芯片的晶振与时钟的问题!

Other Parts Discussed in Thread: CDCE62005

我们参考6678 EVM做的一款带有两个DSP的开发板,上电控制用spartan6。两个DSP分别用了参考EVM板的两组CDCE62005时钟芯片。

今天我在调试DSP1的时候出现了Error connecting to the target:Connect to PRSC failed的问题,然后就去测时钟,发现DSP1时钟芯片的输出波形都不正常,但是DSP2的CDECE时钟芯片的输出时钟完全正常!

我测了时钟晶振,DSP2那组的晶振信号特别好,但DSP1那组的晶振信号不行!我又对比了两组芯片的管脚的电压,发现在连接晶振的管脚处两者电压不一样,不正常工作的那组CDCE芯片的连接晶振的管脚电压是0.05~0.15V之间,正常的那组连接晶振的管脚电压是2.0V,我怀疑晶振没正常工作是因为起振电压不够。

两组时钟用FPGA控制他们工作的程序是相同的,但结果却是一组正常工作,一组不正常工作。那为什么不正常工作的那组CDCE芯片管脚电压是这种情况呢?

再说一下板卡的情况,最初烧写了FPGA控制程序调试的时候,两组芯片都可以正常工作,稳定输出所需要的时钟,然后将FPGA控制程序烧写到板子上依旧工作正常,也正常工作了好久。但是今天DSP1突然出现了Connect to PRSC failed的问题,而DSP2可以正常工作。

想请问TI的员工和论坛的技术大牛们,这种情况是怎么回事,会是晶振坏了吗?还是说连接晶振的那个管脚电压不正常代表CDCE芯片坏了?或者是要从FPGA固件下手!

PS:对于这个两组芯片他们的powerdown信号都是正常的3.3V,而且测试了供电的电压,也都正常!

希望能有人给一个解答,谢谢~