This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于USB3.0

Other Parts Discussed in Thread: TUSB7320, TUSB7340, TUSB8040A, TUSB9261, TUSB1310

最近有个项目关于USB传输的,对传输速度有一定的要求。如果用USB2.0的话,可能会有瓶颈,想用USB3.0,想咨询一下TI的专家,现在TI有没有能够支持USB3.0的平台?

  • 目前TI有一些关于USB3.0的transceiver,由于这些transceiver必须和FPGA搭配使用,TI已经和第三方公司合作开发了关于USB3.0的demo board,使用TI的transceiver和第三方公司的FPGA。您可以联系下第三方公司:

    www.plda.com

    www.slscorp.com

  • TUSB73x0系列芯片可能会是你需要的,这是一个usb3.0 controller

  • 关于USB 3.0的应用,目前TI的产品覆盖很全:

    xHCI USB 3.0 Host Controller: TUSB7320、TUSB7340          //PCI-e ->USB 3.0

    USB3.0 Hub:                                TUSB8040A                               //1:4 USB3.0 Hub

    USB3.0 to SATA Bridge:             TUSB9261                                

    USB3.0 Redriver:                         SN65LVC502/502A        

    USB3.0 PHY :                                TUSB1310

  • TUSB7340出现的问题

    我们用USB3.0 U盘进行文件拷入拷出测试时,有时能拷贝文件,有时不能,且驱动快速不停打印如下信息:

    xhci_hcd 0000:01:00.0: WARN: transfer error on endpoint
    usb 4-3: reset SuperSpeed USB device number 2 using xhci_hcd
    xhci_hcd 0000:01:00.0: WARN: short transfer on control ep
    xhci_hcd 0000:01:00.0: xHCI xhci_drop_endpoint called with disabled ep d6ab7120
    xhci_hcd 0000:01:00.0: xHCI xhci_drop_endpoint called with disabled ep d6ab714c

    跟踪transfer error on endpoint错误,发现是由USB3.0主控器回报的USB transaction error类型错误导致的,3.0规范写到USB transaction error可能由DPP error或者transaction timeout引起,USB 3.0规定,transaction timeout引起的USB transaction error,usb3.0主控器应halt相应ep,ep回应stall信息,主控器回报stall事件,从测试结果看,并没有监控到stall事件,而是不断复位设备。对主控器上电顺序涉及的信号进行了测量,符合上电顺序要求。

    无法断定USB transaction error是由dpp error引起的,该如何解决?

  • 您好,向您请教TUSB7340问题。

    我们用USB3.0 U盘进行文件拷入拷出测试时,有时能拷贝文件,有时不能,且驱动快速不停打印如下信息:

    xhci_hcd 0000:01:00.0: WARN: transfer error on endpoint
    usb 4-3: reset SuperSpeed USB device number 2 using xhci_hcd
    xhci_hcd 0000:01:00.0: WARN: short transfer on control ep
    xhci_hcd 0000:01:00.0: xHCI xhci_drop_endpoint called with disabled ep d6ab7120
    xhci_hcd 0000:01:00.0: xHCI xhci_drop_endpoint called with disabled ep d6ab714c

    跟踪transfer error on endpoint错误,发现是由USB3.0主控器回报的USB transaction error类型错误导致的,3.0规范写到USB transaction error可能由DPP error或者transaction timeout引起,USB 3.0规定,transaction timeout引起的USB transaction error,usb3.0主控器应halt相应ep,ep回应stall信息,主控器回报stall事件,从测试结果看,并没有监控到stall事件,而是不断复位设备。对主控器上电顺序涉及的信号进行了测量,符合上电顺序要求。

    无法断定USB transaction error是由dpp error引起的,该如何解决?

  • 可以看看TUSB1310芯片

  • 请问该问题后续如何解决的?

x 出现错误。请重试或与管理员联系。