This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
ts3usb30e是不能作为串口的切换开关的,因为串口通讯的电平已经超过了ts3usb30e的VCC范围,即ts3usb30e的VCC的范围是3V~4.3V,且此芯片为单极性芯片,而串口通讯中定义+5~+12V为低电平,而-12~-5V为高电平。故不支持使用此芯片做串口的切换使用。
另外补充一点,此芯片一般用于Routes Signals for USB 1.0, 1.1, and 2.0。
你好 我说的串口是单片机的串口,该串口的电平在3.3V不是电脑上的串口。
你好 我还想问下 如果用ts3usb30e作为usb和串口的模拟开关的话,有什么问题么?
Hai,
你好!TS3USB30E可用于USB与UART串口之间的信号切换,只要用于切换的信号电平低于Vcc且带宽不超过900MHz即可,谢谢!
你好,这样的切换你有尝试吗?有什么问题吗?如果不行,你最后采用的是什么方案?谢谢了
Tuanwei 你好:
TS3USB30E虽然定义为USB的二选一开关,但也经常用来做USB及UART之间的信号切换,用于调试的UART信号不会超出USB的带宽,这样使用是没有问题的,谢谢!
切换没有问题,用是是3.3V的单片机串口 USB和串口切换没有问题