利用CDCE72010产生自己需要的频率,对寄存器进行配置,结果一直不正确。手册中说的晶振频率491.52MHz,这个频率是固定不可修改的吗?因为采用二分频输出时,无论怎么配置,输出时钟都是245.76MHZ,请问这种问题如何解决呢,新手求指教!感激不尽!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
利用CDCE72010产生自己需要的频率,对寄存器进行配置,结果一直不正确。手册中说的晶振频率491.52MHz,这个频率是固定不可修改的吗?因为采用二分频输出时,无论怎么配置,输出时钟都是245.76MHZ,请问这种问题如何解决呢,新手求指教!感激不尽!
你的输入输出频率分别是多少?245.76是由内部的VCO分频下来的。看看VCO的分频
491.52MHZ是默认VCXO的值,这个是不可改变的,如果根据你的配置,VCXO不是491,52MHz ,可以使用外部VCXO_IN引脚提供
谢谢你的回复!也就是说默认的频率值不能改变,芯片的输出频率只能配置成491.52MHz的N分频对吗?假如我需要一个240MHZ的输出频率,可以实现吗?