This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN55HVD251: CAN收发单端波形异常原因

Part Number: SN55HVD251

Q1:数据手册中Figure33中,虽然CAN差分波形没有任何异常,但是为什么CANL及CANH刚开始恢复隐性的时候,不是快速的恢复2.5V,而是先快速恢复到2V左右,然后缓慢抬升到2.5V,请提供该波形测试使用的电路,并详细解释该异常波形存在的原因。

Q2:对于数据手册Figure29,提供了一种预留终端电阻的解法,请问如果这个网络中CANL地VREF的电阻不接(即不使用这个网络的终端电阻),请问贵公司有没有测试过CAN总线的单端对GND的波形,这样的接法对总线是否有其他不利的影响。

  • 已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 您好

    Q1:由于驱动器关闭时预期的模拟行为,总线将处于悬空状态并由总线/电缆电容/节点电容/寄生参数等控制,这种情况应属典型。通常需使用2个或更多CAN节点(驱动器+接收器)、两个120欧姆终端(位于总线两端)以及符合数据手册第9.2.1节要求的电缆建议进行测量。

    Q2:是的,这应成为CAN分析中的标准条件。若未连接,共模电压应变得更不稳定。即,无主要直流功能故障/通信问题,反而可能产生额外噪声并伴随一定振荡,谢谢。