Other Parts Discussed in Thread: TXB0104
TXB0104如果只使用两路,剩余两路闲置会不会有影响,如果有影响应该如何处理?
TXB0104输入端上拉应该选择多少?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TXB0104
TXB0104如果只使用两路,剩余两路闲置会不会有影响,如果有影响应该如何处理?
TXB0104输入端上拉应该选择多少?谢谢
没有影响,每路都是独立的。
TXB0104适用于外部不需上拉电阻的情况,如果要加,阻值必须大于50kΩ。如果对于你的应用是open drain情况需要外部上拉,建议看看TXS0104。
不用的IO上拉或者下拉主要保证它们在固定的电平即可。
如需要选择电阻取值,可以根据VCC*Rpull/(Rpull+4k)=Voh进行计算,4Kohm是内部串联的阻值大小。
A测电压是3.3V,B测电压是5V,假如在输入端(A)加一个1K的(3.3V)上拉电阻,VOH是不是A测静态时的电平,按道理我焊接1K的电阻时,A测引脚电平应该是3.3V/5,但是为什么我加了1K上拉,我测着A测电平是3.3V,如果10K上拉是0.9V,还起不到上拉的作用了喃?
感觉公式有点像,3.3*4/(4+RPULL)=VOH。
求解答 谢谢
漏极开路使用TXS系列,如果需要很强的驱动能力,比如驱动阻性负载,建议使用245,125一类的做电平转换。