从SN75DP126规格书上看支持HDMI1.4版本HDMI输出,但是在测试过程中最高分辨率仅在1080@60Hz;
“支持线缆长度为 10 米且 TMDS 时钟频率高达 340 MHz 的 HDMI 1.4b“,这是规格书上的介绍,340MHz的时钟频率完全可以支持4K@30Hz分辨率的;
测试所使用的源和显示设备均支持4k@30Hz分辨率;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.