Part Number: TXS0108E
Why should the n-pass resistor on the TXS0108 be set to around 200 ohms, rather than around 20 ohms as on the TXS0104?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXS0108E
Why should the n-pass resistor on the TXS0108 be set to around 200 ohms, rather than around 20 ohms as on the TXS0104?
Hello,
I did not see the 200 ohm resistor you described in the datasheet.
You can refer to this article to learn about the resistance values of external pull-up and pull-down resistors.
In addition, TI provides development board and reference design, which you can also refer to
Development board:www.ti.com.cn/.../TXS0108E
Reference design:www.ti.com.cn/.../TXS0108E