This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28377D-SEP: F28388D 外设EMIF1地址线A5表现异常

Part Number: F28377D-SEP

我同时在28P65SH7和28388D两个DSP上面使用EMIF功能(异步模式对FPGA通信)。28P65上的EMIF完全正常运行后,我把28P65的配置原样移植到了28388D上面,仅仅调整了PIN口的配置,EMIF的初始化方法完全一样。但是28388的EMIF遇到了问题:PIN口(K19)EMIF1_A5(GPIO45)在DSP写EMIF的时候表现正常,但是在DSP读EMIF时为高电平无法根据数据地址进行高低变化。除此之外一切正常,我刻意使用A5本就为高的数据地址进行读EMIF就可以正常收到数据。所有的地址线和数据线都是直连FPGA没有外部上下拉操作,GPIO部分配置了地址线为输出模式。

我尝试把这个口配置为GPIO45,写1写0正常,配置为EMIF1_A5后写EMIF正常,读EMIF异常。

请问怎么排查这个问题?