看到TI DS90C187有single pixel in/dual link out mode 不知道能否很好的支持1280*1024,60HZ的液晶屏 ?
我用的OMAP3530 ARM 模块输出的信号是24bit ttl 要接双通道的LVDS屏,AUO G170EG01V0 分辨率1280*1024,标准刷新率60HZ.
需要有论证以往下看是实际验证还是重新考虑芯片选型。谢谢您的支持与信任!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HOR PIXELS 1,280
VER PIXELS 1,024
HOR FREQUENCY 63.668
ACTUAL VER FREQUENCY 59.895
PIXEL CLOCK 109.000 MHz
可以使用DS90C187,在single pixel in, dual pixel out 情况下可以pixel clock 最高可以到185MHz.