This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询专家: 关于用xio1100 PCIe 桥芯片,设计 PCIe 转 canbus 的方案

Other Parts Discussed in Thread: XIO1100, ISO1050

 

我们需要开发PCIex1CANBUS 板卡,初步选定TIXIO1100作为接口芯片,整个板卡的的大致实现:
1,用XIO1100转为TI-PIPE MAC Interface。
2,选择一款ARM cortexM3或者M4,或者C2000,与XIO1100的TI-PIPE MAC Interface对接,利用cortexM3或者M4,或者C2000内部的CAN控制器实现CANBUS;
3,用ISO1050 隔离CAN收发器实现CANBUS传输。
 
请问:
1,目前很多方案都是用FPGA芯片与PCIE桥接芯片如XIO1100对接,在这个PCIex1CANBUS这个项目中,选用cortexM3或者M4,或者C2000,与XIO1100对接是否能够实现,或者根本就不能实现,如能实现请推荐一款TI的 cortexM3或者M4,或者C2000芯片。想优先考虑cortexM3或者M4,或者C2000的原因是不想花太多的时间去做FPGA.
2,XIO1100是否有相应的开发工具,如demo板等,以加快开发进度。
 
vikenzhou
13611914418
email: viken@126.com
QQ:40366143
 
 
 
 

 

x 出现错误。请重试或与管理员联系。