This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RS485 SN65HV12D接收无效数据

在使用SN65HV12D搭建RS485电路时,将RE和DE短接,发现如下现象:

1.不发送数据时,TX无数据输入,一直保持高电平;RX也无数据输出,一直保持低电平。

2.发送任意数据时,TX为正常数据输入;有的电路板RX无数据输出,一直保持低电平;有的电路板RX有00(16进制)数据输出。

正常电路板TX与DE示波器截图如下

正常电路板RX与RE示波器截图如下

问题电路板TX与RE示波器截图如下

问题电路板RX与RE示波器截图如下

电路原理图如下,R20未接,R21短接