This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI83: SN65DSI83上电偶发横向周期性闪烁

Part Number: SN65DSI83

Hi Ti Team,

我们设备采用的MIPI->LVDS方案,选的SN65DSI83芯片。

目前现象:

偶发上电屏幕横向周期性闪烁(横向撕扯的现象,横线撕扯马上又恢复正常,然后0.5s~1s立马又出现横向撕扯,如此周期性重复)。而且一旦上电出现闪烁,会一直存在,不会自动消失。如果上电没有出现闪烁,后续不会出现闪烁。

屏幕参数:

clock frequency: 74284800Hz

H-Active: 1280

V-Active: 800

H-back porch: 88

H-front porch: 72

H-sync-len: 20

V-back porch: 23

V-front porch: 15

V-sync len: 10

试过改动过back porch/front porch/sync len/clock frequency,都无法解决。

做过的测试:

1.在横向闪烁的时候,通过IIC切换SN65DSI83到测试模式,屏幕没有出现闪烁,再切回正常模式,又恢复横向闪烁;

2.在横向闪烁的时候,通过IIC设置PLL_EN到disable再到enable,屏幕黑屏后会恢复到正常显示界面(没有闪烁);如果多次切换PLL_EN disable/enable,会偶发出现屏幕闪烁现象。

3.在横向闪烁的时候,通过IIC设置CHA_SYNC_DELAY,设置奇数的时候,屏幕不闪烁,设置偶数的时候屏幕出现横向闪烁。

重新上电复现横向闪烁,通过IIC设置CHA_SYNC_DELAY,设置偶数的时候,屏幕不闪烁;设置奇数的时候,屏幕出现横向闪烁。

4.再横向闪烁的时候,带电重新插拔LVDS排线,存在50%的概率屏幕恢复正常(不闪烁)。

5.更改LVDS屏幕的各种设置以及复位时间,VGH/VGL时序,均不能解决闪烁现象。而且在出现上电横向闪烁的时候,屏幕自带的VGH和VGL均出现周期性跌落现象,VGH(VGH=18V)的跌落幅度在5~7V左右,VGL(VGL=-10V)的跌落幅度在3~5V左右。

请问一下,出现这种横向闪烁,需要怎么排查解决?