This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在一个项目用到了CDCE937这款芯片,但遇到一点点问题,请教下:
1)烧写时CLOCKPRO里怎样进行设定。
2)生成的HEX,可以直接用通用烧写器进行烧写吗?
3)S0S1S2与芯片上电的关系如何。
谢谢!
看上去应该是通过ClockPro和CDCEL9XXPROGEVM编程板来实现对CDCE937的烧写。但是不确定能否直接用ClockPro驱动通用烧写器,你可以试试看。生成的.HEX文件应该可以直接导入通用烧写器。
你好!
CDCE937的寄存器配置只能通过SPI通讯来进行配置的,即朝EEPROM写配置的,使用通用烧写器应该是无法通过SPI通讯来完成烧写的,目前接触的基本上都是使用单片机来完成朝寄存器里写配置的。
详细的可参考CDCE62005EVM上的参考电路。
S1/SDI,S2/SDO是复用数据线,S0s1s2主要是用于pin-control模式,即可以直接通过端口设置来控制EEPROM相关寄存器的参数,详细可参考page10-11,而其默认的是SPI通讯模式的SDI和SDO。