This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD234: LAUNCHXL-F28379D 控制板can通信问题

Part Number: SN65HVD234
Other Parts Discussed in Thread: LAUNCHXL-F28379D,

尊敬的先生/女士,您好:

我在使用贵公司的LAUNCHXL-F28379D控制板进行can通信,我的程序基于simulink MBD 开发模式中,现在无法实现can通信,现象如下:

1.我在simulink中canb里选择self mode test模式,可以在上位机中看到数据,但仅限于can transmit;

2.我在canb 中不选择self mode test 模式,在上位机中can通信的收发都失败;

3.我使用贵公司2879xd中can 例程中的can transmit/receive,寄存器中显示bus-off;

4.我对SN65HVD234芯片的EN引脚排查,发现电压为1.87V,怀疑芯片处于休眠模式,我对该EN引脚飞线处理拉高到3.3V,can通信仍然失败;

5.SN65HVD234芯片的1引脚和4引脚一直处于拉高状态,CANH/L引脚之间的电压差为0,电阻正常;

我现在的疑问是,can通信为何失败,是收发器损坏吗?

期待您的回答,谢谢!