DS560DF410: About DS560DF4100 output swing

Part Number: DS560DF410

Hi team,

A 12.4416Ghz input signal to the Rx channel.We configured for 24.8832 Gbps NRZ PRBS7 with a differential swing of 1000 mV using the opcodes given below. however, the measured output is only 200 mV and Bit rate is 24.8832Gbps .We have tried tuning the FFE (opcode 0x0C), yet it still stays at just 200 mV. Do you have any suggestions or troubleshooting steps to resolve this?

 

WIIC 0X30 0X0 0XA2

RIIC 0X30 0X64

after 500

 

//opcode 0xD2

WIICS 0X30 0X3C 14 0x04,0xA8,0x61,0x0,0x0,0x0,0x1,0x00,0x1F,0x0,0x00,0xB0,0x7B,0x1

WIIC 0X30 0X3B 0XD2

RIIC 0X30 0X64

after 1000

 

//opcode 0x61

WIICS 0X30 0X3C 3 0x04,0x1,0x0

WIIC 0X30 0X3B 0X61

RIIC 0X30 0X64

afeter 500

 

//opcode oxC6

WIIC 0X30 0X3C 0X04

WIIC 0X30 0X3B 0XC6

RIICS 0X30 0X6C 2

  • Hello, we have received your case and the investigation will take some time. Thank you for your patience.

  • 你好,

    对于延误,我们深表歉意。我将在本周末前回复您,并提供后续步骤的建议。

    此致,

    格雷格

  • 你好,

    这个问题是否存在?如果存在,该设备是否实现了CDR锁定?输入时钟是什么?

    此致,

    格雷格

  • 你好, 我们在增加Tx_LUT的配置后,输出幅度正常。 但是目前我们遇到了新的问题,我们在参考如下步骤进行误码测试时,调制方式是NRZ时可以测试到无误码状态, PAM4方式无法测到无误码状态,使用Latte上脚本方式PAM4是可以测试到无误码的,可以确定硬件环境能满足无误码条件 RX端确认CDR处于LOCK状态 TX LUT和RX LUT已经正确配置 另外尝试手动调整了CTLE和PLL 误码测试步骤如下 This macro is needed for getting BER measurement using internal PRBS module. To do the BER measurement following macro sequence needs to be followed. 1. Exit background calibration with 'Stop background calibration optimal' (see Section 4.3.54; use Operand2: BER). 2. Confirm background calibration exit with 'Execution status' macro (opcode: 0x37; see Section 4.3.36) , issue this macro multiple times till it returns '1'. 3. Configure BER module (opcode: 0x62; see Section 4.3.27). 4. Enable BER module (opcode: 0x63; see Section 4.3.28). 5. Measure BER with 'Get BER' macro (Section 4.3.30) or with '*** Error Readback' (Section 4.3.46). Former one is a blocking macro which gives BER over a fixed window size. Later one gives the BER till now.. 6. Optionally, restart background calibration with ‘Stop background calibration optimal’ (see Section 4.3.54) operand 2: 0x00

  • 你好,
    我们在增加Tx_LUT的配置后,输出幅度正常
    但是目前我们遇到了新的问题,我们在参考如下步骤进行误码测试时,调制方式是NRZ时可以测试到无误码状态
    PAM4无法测到无误码状态,使用Latte上脚本方式PAM4是可以测试到无误码的,可以确定硬件环境能满足无误码条件
    RX端确认已经处理LOCK状态
    TX LUT和RX LUT已经正确配置
    另外尝试手动调整了CTLE和PLL,均无法测试到无误码状态

    1、对于测试环境满足无误码条件时,PAM4的误码检测在如下步骤下是否需要增加其他额外的配置才能测到无误码?如果有,具体是什么?如果没有,是否有其他配置建议解决无法测到无误码的问题?

    2、芯片的误码计数器实际可以满足较大误码率测试,我们实际最大误码率只能测试到1E-5左右,如果需要测试到大于1E-5的误码率,我们对应可以优化配置的方向是哪些?

    期待你的回复

    误码测试步骤如下
    This macro is needed for getting BER measurement using internal PRBS module. To do the BER measurement
    following macro sequence needs to be followed.
    1. Exit background calibration with 'Stop background calibration optimal' (see Section 4.3.54; use Operand2:
    BER).
    2. Confirm background calibration exit with 'Execution status' macro (opcode: 0x37; see Section 4.3.36) , issue
    this macro multiple times till it returns '1'.
    3. Configure BER module (opcode: 0x62; see Section 4.3.27).
    4. Enable BER module (opcode: 0x63; see Section 4.3.28).
    5. Measure BER with 'Get BER' macro (Section 4.3.30) or with '*** Error Readback' (Section 4.3.46).
    Former one is a blocking macro which gives BER over a fixed window size. Later one gives the BER till
    now..
    6. Optionally, restart background calibration with ‘Stop background calibration optimal’ (see Section 4.3.54)
    operand 2: 0x00