This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC16244A单输入多输出问题

Other Parts Discussed in Thread: SN74LVC16244A, CDC318A

你好

我们用MCU产生一路500KHZ~1MHZ频率的clock信号,需经buffer扩展为13路输出,给后级的多片DC/DC控制器做同步时钟。

Buffer打算用SN74LVC16244A或类似器件,但这类buffer IC一般是input-ouput一对一的,是否可以将同一个信号源接到13路input?

不太清楚此类buffer器件对输入信号是否有明确的驱动能力要求?主要是担心MCU输出能力不够,无法同时带动SN74LVC16244A的13路输入。

当然也可以用cdc318a等专用时钟buffer IC,但成本过高。

另外,此类逻辑器件的功耗应如何估算?一般是频率越高功耗越大,但希望了解比较合理的估算公式。

谢谢!