你好,我司目前在使用DS100DF410, 目前通过I2C配置的方法已经搞定了信号的问题。
问题,我们现在需要设置成不是通过i2c来配置,而是读取EEPROM配置的方式。目前我们的设计是一颗DS100DF410对应一颗EEPROM.
我们把READ_EN接地,EN_SMB浮空,SDC没有信号输出,一直为高,ALLDONE也是高。
也尝试过READ_EN从高变成低,SDC依然没有信号输出。另外也尝试了把READ_EN从高变低,再变高。SDC还是没有信号输出。
想问一下,DS100DF410需要什么条件才会去从EEPROM里面读取数据? datasheet描述是从高变低。而snlu126b这份文档的4.3.1.1上面说只要接地就可以。demo原理图的第一颗DS100DF410也是READ_EN接地。