This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVCH16T245 partial-power-down问题

Other Parts Discussed in Thread: SN74LVCH16T245

你好

请问

(1)SN74LVCH16T245在VCCA或VCCB只有一个电源有电的情况下,输出为高阻吗?

This device is fully specified for partial-power-down applications usingI off .The Ioff circuitry disables the outputs, preventing damaging current back flow through the device when it is powered down

(2)假设方向为A-->B(3.3V转5V),某种工况下VCCA电源失电,但A侧输入有电压,器件是否会损坏?如果不会,输出为高阻?

谢谢

  • 1)The VCC isolation feature ensures that if either VCC input is at GND, both ports are put in a high-impedance state.只有一个电源,输出为高阻。

    2)不会损坏,输出为高阻。

x 出现错误。请重试或与管理员联系。