This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教专家: SN74AVC4T245 和SN74AVCH4T245 有啥区别?

Other Parts Discussed in Thread: SN74AVC4T245, SN74AVCH4T245

我设备是1.8V的GPRS模块,MCU是3.3V。 以前一直是用的SN74AVCH4T245。这次供应商疏忽发成了SN74AVC4T245 。我怕使用有问题,又找不到两者的大区别别。请专家解释一下两款芯片的最大区别。 用混了有啥不良后果。谢谢了!

  • SN74AVCH4T245中的H意思为bus-hold 。说明这款器件带有总线保持电路,简单来说,就是可以维持输出在一个有效的逻辑电平内,即使输入是一个无效的逻辑状态,通常情况下,不带总线保持功能的,不建议输入端直接悬空,我们需要上拉或下拉使得输入端在一个有效的逻辑电平内,而这种则不需要上下拉:

    Active bus-hold circuitry holds unused or undriven inputs at a valid logic state. Use of pullup or pulldown resistors with the bus-hold circuitry is not recommended.


x 出现错误。请重试或与管理员联系。