This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
为什么ISO3082 通讯的时候会多个零出来额
通讯要保持电平匹配
通讯出现乱码?建议详细描述下你目前的情况,或者把电路图发过来看看。
iso3082 在切换到数据发送时,需要插入延时吗? 能否立即发送数据?使用的是主频72MHz的ARM 引脚翻转速度50MHz
需要注意ISO3082的data rate只能支持到200Kbps。你目前的数据data rate多少?
我用的波特率是9600,我的意思是我在做485通信的时候,接收是正常的,就是在发送数据时,使能了DE后立即发送数据,开始几位数据不对,而且多出几位!软件机制在其他485通信方案中是可以的,
问题解决了,是USB转485的问题!