This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04906用法

Other Parts Discussed in Thread: LMK04906

我想利用LMK04906得到一对差分的正弦波输出,正弦波基频大概只有10K~30k,然后使用一个性能优良的低通滤波器得到基频信号,不知道是否能够实现,正弦波信号的动态范围能否达到一定的精度,比如说100dB以上,阅读了LMK04906的datasheet,上面介绍了该芯片接受1Khz到750Mhz的时钟输入,并生成2.26Mhz到2.6Ghz的输出频率,我想是否能够输出频率更低的的信号,如果该芯片不能满足需求,是否可以推荐一款芯片,让我可以完成一个高精度正弦波发生器的设计,要求动态范围可以达到100dB,正弦波输出经过频谱仪可以得到的SNR也在90dB左右