This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XC3S200AN通过I2C对CDCL6010芯片进行配置,CDCL6010的I2C不输出应答。

Other Parts Discussed in Thread: CDCL6010

板子上有两片CDCL6010,XC3S200AN通过I2C对它们进行配置,XC3S200AN是I2C主设备,两片CDCL6010是I2C从设备,地址分别设置为00与01。XC3S200AN的I2C接口逻辑简单仿真是对的,chipscope抓的输出的波形也没有问题,就是收不到CDCL6010的应答位,两片CDCL6010都收不到,接下来不知怎么调了。

  • I2C从机地址不对啊,7位从机地址11010 ADD1  ADD0,所以一共可以接4个设备,分别为1101000, 1101001, 1101010和1101011。

    所以地址为00和01肯定不对,导致不能收到ACK信号。

  • 谢谢回复。这里的00、01是不包括11010这5位固定部分的。

    问题找到了,一是按照6010手册中scl加了一个电容,可能容值选的有点大,后来直接焊下来了;二是I2C的接口程序有问题,试了几个不同的程序,后来就可以了。I2C接口代码xilinx没有IP核,只能参考其他的代码。

  • 谢谢你的反馈,也很高兴你的问题得以解决。